Site Survey
After you have created a project, the next step is to gather information about the source system to start the migration process. The site survey has detailed questionnaire that gathers necessary site data.
The site survey is not a compulsory task but is a task which is advised to perform.
Click on
icon.
A new window appears as shown in the figure below. Click Continue.
There are eight more pages of data to fill. Fill the data and click Submit.
This completes the site survey task.
Proceed to import PLC5 or SLC 500 files from the source system.