Create a New Project
You can create a new project only if you have access to log in to the ControlEdge Transition.
Perform the following steps too create a new project:
-
On the dashboard, click
and Enter Project Details
window appears.
-
Enter Project Name: Enter the name of the project in 32 alphanumeric characters or less. Make sure not to enter any symbols.
-
Enter Project Description: Provide a brief description of the project in 256 alphanumeric characters or less. Make sure not to enter any symbols.
-
Enter Site Details: Provide useful information about the site in 256 alphanumeric characters or less. Make sure not to enter any symbols.
-
Select Region: Select geographical region of the site. Select one of the regions from available from the scroll down menu.
-
Assign User: This option is filled automatically. Thus you don't have to select anything on this option.
-
Select Source System: Select the source system. Currently, PLC 5 and SLC 500 are the only systems supported.
-
Select Target System: Select the system the customer desires to migrate. Currently, ControlEdge PLC 140, ControlEdge PLC 150, ControlEdge PLC R151, and ControlEdge PLC R160 are the only systems supported.
-
Click Create. The dashboard appears with your new project.
-
On the dashboard, hover your mouse over the project you just now created and click
to view the details
of your project. You will see all the details you entered when creating
this project on the top.
Status completion is shown as 5%.
You may have to scroll down to view the newly created project if there are already four or more projects on the dashboard.